The Charging Point CP001/002/003 is the connection between power and your application. It is designed to fit into all designs and comes in three different versions.
The CP001 is a simple cable with a jack plug that gets connected directly to the power cable. This charging point is very discreet and compact.
The CP002 also comes with a jack plug and has a light indicator that lights up when the system is connected to power.
The CP003 is a magnetic charging point that has a light indicator, which lights up when the system is connected to power. The magnetic function protects the application by snapping apart if the charging cable is being pulled.
The Charging Points CP001, CP002 and CP003 are designed for an intuitive use when connecting your application to power.
A safety release cable is optional for CP001 and CP002. It protects the application by snapping apart if the charging cable is being pulled.
View the data sheet as an online magazine or download the PDF.
This user manual will explain how to pair, set up and use the LA10 system for recliners.
Explore the variety of HOMELINE systems and products for both adjustable beds and recliners.
Explore our reliable actuator systems for adjustable recliners with a wireless control unit. We conducted research to make sure that this system takes the entire value chain into consideration.
Recliner - How do I assemble the LA10 system for recliners without a battery?
Learn how to assemble the LA10 actuator system for recliners without a battery.
The system in the video consist of the following:
For more information about the LINAK® Recliner system, please visit the recliner application page.
Recliner - How do I know if my recliner has a LINAK system?
Learn how to see if your recliner has a LINAK® system.
You can usually see if a system is produced by LINAK by looking at the SMPS or under the batteries in the hand control.
Recliner - How do I mount the Charging Point in a recliner?
Learn how to mount the charging point CP002 and CP003 in a recliner with LINAK® systems.
For more information about the LINAK Recliner system, please visit the recliner application page.
Recliner - How do I pair the BP10 control with a recliner?
Learn how to pair the BP10 control to a recliner with a LINAK® system.
For more information about the LINAK recliner system, please visit the recliner application page.