Contact us here
Controls

DPG with reminder

DPG1M, DPG1B and DPG1C are a family of intuitive LINAK® Desk Panels operated by a gentle tilt. They come with Bluetooth® wireless technology, memory and reminder functions.

Desk Panels DPG – Designed to shape behaviour play-icon

Desk Panels DPG – Designed to shape behaviour

Office worker sitting at a sit-stand desk using the LINAK Desk Control app play-icon

Use your sit-stand desk better with Desk Control App

Engineer working on a LINAK office desk play-icon

I am LINAK

DPG with reminder

DPG desk panel models with reminder 
The DPG with reminder family consists of DPG1M, DPG1B and DPG1C Desk Panel models. All DPG models are activated by tilting; an easy intuitive way to adjust a desk without any attention needed. With the DPG, you get up to four memory positions which are reached by simply tilting the panel until the desk stops at the stored position. 

The colour indicates to the user to change position
The integrated reminder function of the three DPG Desk Panel models is visualised by a light. Its colour reflects the current usage status of the desk. A colour change of the light reminds the user when it is time to change position. The reminder function thus naturally supports the user to achieve a healthy posture variation throughout the day.

Compatible with the Desk Control™ app
DPG Desk Panel models with a reminder function are compatible with the Desk Control app, using the integrated Bluetooth® wireless technology. The app allows the user to keep track of his personal desk usage statistics on a smart device and get notifications when to stand. 

 

DPG1C data sheet

View the data sheet as an online magazine or download the PDF

DPG1M data sheet

View the data sheet as an online magazine or download the PDF

DPG1B data sheet

View the data sheet as an online magazine or download the PDF

Desk Panels DPG and Desk Control app user manual

This user manual will tell you how to install, use and maintain your LINAK DESKLINE® products.

DESKLINE product overview

If you make any kind of desk, table or counter that people work behind, a height adjustable electric actuator solution is the flexible way to gain a competitive edge and improve your business.

MOVE – Why sit-stand desks increase work performance

Reduce sick days and create a modern office environment with electric sit-stand desks. An attractive investment for employers and their employees.

Desk Panels DPG - the innovative way to adjust office desks

This intuitive desk panel series is designed to shape behaviour and is operated by tilting. Advanced models offer visual sit-stand reminders, height memory, Bluetooth® connectivity and much more.

Desk Control™ App - Can I combine the use of the app on more devices at the same time?

No. There is only one Bluetooth® connection on the DPG. So only one device can be connected at a time to the DPG. The device (either your mobile or your computer) that first connects with the DPG will be the device on which you can use the app.

Desk Control™ App - I cannot find the Desk Control App in the Windows Store. Why is that?

The Desk Control App for Windows is only available for Windows 10 in the Microsoft Store. If you have an older Windows version, you cannot download the Desk Control App.

Desk Control™ App - My desk drives only a few centimetres, then it stops. Why is that?

Your Bluetooth® driver may be outdated. Ensure that the latest Bluetooth driver is installed on your computer.

Desk Control™ App - What is the difference between connecting as “Owner” and connecting as “Guest”?

The difference is where your personal settings are stored and whether you are automatically reconnected to the desk.

If you connect as “Owner”, your reminder and favourite settings are stored in the DPG on the desk and your app will automatically connect to this desk when you arrive at it and track the statistic sit/stand data throughout the day.

If you connect as “Guest”, your reminder and favourite settings are stored on the app on your smart device/computer and when you connect to a desk, these settings will reflect in the DPG. You need to pair the app with the desk every morning and then for the rest of the day the app will automatically connect to this desk and send standing notifications and keep track of sit/stand data.

Desk Control™ App - Who can access/use the data?

The data can only be accessed in your device. LINAK does not access or use any data entered in the app (such as favourite positions, height, weight, and gender) or collected by the app (statistics).

Desk Control™ App - Who owns the data entered in/collected by the app?

The user owns all data entered in/collected by the app. Delete the app to delete all data. Go to settings on your device to delete the app. If you re-install the app, you need to pair the app and the desk again to be able to control the desk via the app.

Desk Control™ App - Why can I not operate my desk with the app?

You can use the app if your desk has Bluetooth® connection. The Bluetooth connection happens via a DPG desk panel with reminder (all app versions) or a BLE2LIN adapter (iOS, Android and Windows 10). If you have a DPG without Bluetooth, you cannot use the app.

Desk Control™ App - Will the app keep collecting data if I am not at the desk?

The app detects if the smart device/computer is close enough to the desk to be connected to it. The app will collect data if the connection between the smart device/computer and the desk is established, even if you are not at your desk.

As long as your computer is within reach of the DPG Bluetooth® connection and you are logged into your computer, your standing time is counted in. When your computer is in standby mode, or you have locked the screen, standing time is not counted in.

Desk Control™ App - Will the app remind me to stand if I am not at my desk?

The app detects if the smart device/computer is close enough to the desk to be connected to it. The app will only send notifications if the connection between the app and the desk is established.

How to clean your desk panel

Watch and learn how to easily clean your LINAK desk panel/switch in this short instruction video: How to clean it; which cleaning agents to use; and, last but not least, what you need to pay attention to.

Clean your desk panel with a soft damp cloth. Universal cleaning detergents may be used.

To disinfect the desk panel, use a 70% isopropyl alcohol either as a wipe or add a small amount to a soft cloth.

Warnings
The desk panel is not a sealed unit and there are electronics inside it. If liquids or moisture get into an opening, the PCB may be damaged, and the desk panel ruined.

So:

  • Avoid moisture penetrating any openings as this may damage the PCB inside the desk panel
  • Avoid spraying the cleaning agent or disinfectant directly on the desk panel as moisture may penetrate openings, damaging the PCB inside the desk panel
  • Cleaning agents and disinfectants must not be highly alkaline or acidic (pH value must be 6 to 8), and they must not contain bleach or chlorine
  • Do not use hand sanitiser gel as a cleaning agent

Alkaline and acidic cleaning agents may, over time, decompose the housing. Hand sanitiser gel may deposit on the desk panel buttons. Over time, the buttons may get stuck, or they may not work properly.

Desk Panel DPG1M - How to initialise and adjust the desk

To initialise the desk, drive downwards, press and hold the tilt until movement has been performed.

To adjust the desk, tilt the panel down for driving downwards and up for driving upwards.

Desk Panel DPG1M - How to pair to an app

Press the Bluetooth® button for two seconds. 
The LED starts to flash with a blue colour.

Open your downloaded app and connect to the desk.
Look for your desk in the list of “Desks nearby”.

The LED will flash in a blue colour when connected.

Follow the onboarding instructions in the app.

Desk Panel DPG1M - How to reset the Desk Panel

There are three reset options:

  1. Reset of memory positions
    Press and hold the “star” button for eight seconds until the LED flashes red
  2. Reset of the LED light reminder
    Press and hold the “bell” button for eight seconds until the LED flashes red
  3. Factory reset
    Press and hold the “bell” button and the “star” button for eight seconds until the LED flashes red.
 

Desk Panel DPG1M - How to use memory and automatic drive

To store a memory position drive to the required position.
Press the “star” button for two seconds.
White light flashes and becomes static when the position is saved.

Tilt and hold to drive to a memory position

Automatic drive between two memory positions
(If your desk panel features automatic drive)

Enable automatic drive in the Desk Control™ App.
Tap the desk panel twice in the direction you want to drive.
The desk drives automatically to your stored position.

To reset all memory positions, press and hold the “star” button for eight seconds until the light flashes red.

 

Desk Panel DPG1M - How to use the LED light reminder

The light reminds you when it is time to stand up. 

Green = OK
Orange = It is time to stand up

Set individual goals or deactivate reminder
The default setting is a reminder after 55 minutes of sitting.

Set your goal
Interval 1: Reminder after 55 minutes sitting
Interval 2: Reminder after 50 minutes sitting
Interval 3: Reminder after 45 minutes sitting
Interval 4: Disable reminder

Change the interval by pressing the “bell” button.

How to reset the LED
Press and hold the “bell” button for eight seconds until the LED flashes red.

 

Desk Panel DPG1C - How to initialise and adjust the desk

To initialise the desk, drive downwards, press and hold the tilt until movement has been performed.

To adjust the desk, tilt the panel down for driving downwards and up for driving upwards.

Desk Panel DPG1C – How to pair to an app

Press the Bluetooth® button for two seconds. The light strip starts to blink with a blue colour. The display shows the ID of the desk.

Open your downloaded app and connect to the desk. Look for the correct ID in the list of “Desks nearby”. 

Follow the onboarding instructions in the app.

Desk Panel DPG1C – How to store up to four memory positions and how to reset memory

The DPG with display has four memory positions in total. 

Drive to the required desk height and then toggle the “star” button until the display shows either “star 3” or “star 4”. Release button. 

To store a position press the “star” button for two seconds. White light flashes and becomes static when the positon is saved.

To reset all memory positions press and hold the “star” button for eight seconds, until the light flashes red.

Desk Panel DPG1C – How to use memory and automatic drive

To store a memory position drive to the required position.
Press the “star” button for two seconds. 
White light flashes and becomes static when position is saved.

Tilt and hold, to drive to a memory position.

If the DPG features automatic drive, tap twice on the DPG in the direction you want to drive. The DPG stops at the first stored position in the chosen direction. 

 

Desk Panel DPG1C – How to use the LED light reminder

The light strip reminds you when it is time to stand up. 
Green = ok 
Orange = it is time to stand up

Default setting is 55 minutes sitting. 
Press the “bell” button to see the interval.
 
How to change interval or choose “OFF”. 

Change your interval by toggling between the four settings.

Interval 1: Reminder after 55 minutes sitting

Interval 2: Reminder after 50 minutes sitting

Interval 3: Reminder after 45 minutes sitting

Interval 4: OFF disable the function

How to reset the light strip reminder.

To reset the light strip reminder press and hold the “bell” button for eight seconds until the light flashes red. 

Desk Panel DPG1C – How to reset the Desk Panel

There are three reset possibilities:

  • Reset of memory positions
  • Reset of light strip reminder
  • Factory reset

To reset all memory positions, press and hold the “star” button for eight seconds until the light flashes red.

To reset the light strip reminder, press and hold the “bell” button for eight seconds until the light flashes red.

Factory settings: 
To return to factory settings press and hold the “bell” button and the “star” button for eight seconds until the light flashes red.

Desk Panel DPG1C – How to set the correct desk height. How to change between inch and cm.

Set correct desk height: 
If the height shown in the display is not the actual height of the desk, it can be corrected.

Measure the height of the desk from floor to tabletop. Press the “bell” button and the Bluetooth®  button for five seconds. When the display starts to blink, tilt the panel upwards if the number is too low or downwards if the number is too high.  

Change between cm and inch:
Change between cm and inch by pressing the “star” button and the Bluetooth® button for five seconds. When the display starts to blink, tilt the panel up or down and the unit changes.

The desk can only be lowered

The desk needs to be initialised.

Follow the procedure shown in the video.

The desk cannot be raised or lowered

Possible problem: Mains not connected to the control box
Try/Solution: Try to connect a lamp or similar to the mains supply to check whether there is adequate supply voltage. 

Possible problem: Are plugs mounted correctly in the control box or to the leg?
Try/Solution: Check all connections. 

Possible problem: Are there any visible damages on cables, controls, the control box or legs?
Try/Solution: Damaged parts must be exchanged. Contact the company that sold you the desk. 

The desk cannot be raised full stroke. Always stops in same position.

The system has set a new end-stop outwards.

To reset a saved position, the desk must be re-initialised. Follow the procedure shown in the video.

The Bluetooth® word mark and logos are registered trademarks owned by Bluetooth SIG Inc. and any use of such marks and logos by LINAK® is under license.

Got a question?

Our team is ready to assist you with technical information, starting a project and more.

Contact now

LINAK News

Stay up to date on linear actuator technology

Subscribe