Every year approx. 3,000 people in Denmark die because of an infection they have acquired in hospital. This figure is 18 times higher than the number of people who die in traffic. In the regional hospital in the Danish city of Horsens, they are trying to change this.
The fight against dangerous bacteria
Welcome to the long corridors in the basement of the hospital where the tour starts. This is where the hospital’s service staff work to make daily operations run smoothly. Behind two of the doors is the hospital’s wash tunnel, an advanced automatic wash system that cleans everything from beds to ceiling sheets in the operating rooms. The wash tunnel is just one of the many initiatives the Regional Hospital is taking to increase hygiene.After 17 years in the cleaning industry within hospitals and slaughterhouses, Søren Møller became Service Manager at the Regional hospital in Horsens, where he was worked for the past 21 years. He made the decision to buy the wash tunnel in 2015.
”It all started with the establishment of a manual washing system, and everything was ready. When we had hung up the bed, it was clear that manual washing could not be done satisfactorily and we started to think of machines,” says Søren Møller and continues:
”We put out a tender, in which we specified our requirement for the amount of water, soap, electricity and the wash time based on 15,000 washes a year. We compared the various results and, of course, we chose the one that made the most sense. We are excited about the opportunities it opens and many other regions and hospitals have since come to see the wash tunnel.”
High demands for washability
When Søren Møller started to investigate the market, he was really only looking for a bed washer. But, it soon became clear to him that the new machine could be useful in many more areas. That is when the hospital decided to invest in another machine in line with the hospital's expansion.
”There is focus on the fact that future aids and materials are machine-washable because this makes them much cleaner. The machine cleans many of the things that were previously uncleaned or were cleaned by hand. Today we wash several different things in the wash tunnel, and it will definitely evolve once another machine is up running”.

The beds at the Regional Hospital in Horsens are equipped with actuator systems from LINAK so that they can be adjusted to the needs of the individual patient. Other aids are also equipped with the systems and, as these aids are incorporated in the wash tunnel, more demands are placed on future solutions chosen by the hospital, stresses Søren Møller.
”It is an absolute must that LINAK thinks washability into the systems. We would not buy the beds or aids on which patients are placed if they were not washable. All items on the bed must be able to be washed in the wash tunnel, otherwise it will not work. Previously, the bed was washed by hand, but it was difficult to achieve a satisfactory result. So, from a hygiene point of view, it is clearly a huge advantage when our equipment can be washed in the wash tunnel,” he says, and elaborates:
”It is a legal requirement that hygiene is in order. We work according to the patients' safety in hospital, where there is a major focus on not passing on avoidable infections to patients. That is why we also follow the National Infection Hygienic Guidelines from the Danish Research Institute under the Danish Ministry of Health (Statens Serum Institut). For example, we review 250 rooms four times a year in accordance with INSTA800, which is a common Nordic standard for measuring cleaning quality. This helps us ensure that the cleaning is in order.”
Greater focus on improved hygiene
But, Søren Møller does not only see major hygiene benefits when washing beds and other aids. At the hospital in Horsens, the cleaning is carefully delegated to different areas of responsibility among the service and care staff. It requires both parties to be constantly aware of who is responsible for what. This helps ensure that everything is resolved satisfactorily and that the care personnel staffing is managed sensibly.The main difference, Søren Møller has seen over the past 10 years, is the increased focus on improving hygiene in hospitals. ”Today one thing I always bear in mind when deciding to buy is whether things can be cleaned. We must be able to clean all nooks and crannies efficiently. Otherwise, they are not suitable for use in a hospital,” Søren Møller concludes.
Søren Møller – Service Manager
Washability at LINAK
As a developer and manufacturer of world-class electric actuator systems for hospital applications, LINAK commits to participate in the fight to help hospitals improve hygiene.
Naturally, LINAK actuator solutions meet all international norms and standards for washability. However, some of our products meet an even higher standard because we test significantly more than the 2017 norm prescribes.
We call this stringent requirement LINAK IPX6 Washable DURA™.