Contact us here
Case story

Automation of Sulky fertiliser spreader

LINAK actuators play a large role in many applications involving precision farming. For example, only by an exact and automated regulation of slide controls can fertiliser mixtures be administered accurately.

Automation of fertiliser spreader case story
With Econov, the time for opening and closing the shutter slide on the field boundary side of the X40 or X50 centrifugal fertiliser control can be regulated automatically. Optimisation of the work width can be done in real time.

No more manual control by eye - time for precision!
For this purpose, the machine is connected to a tracking device of the latest generation, as well as a GPS antenna to determine its location in the field.
Through close collaboration, LINAK and Sulky F&E have succeeded in automating all the control processes involved with fertiliser spreaders, using multiple integrated LINAK electric actuators and a connection technique developed by Sulky.

Opening and closing of the intake and the regulation for the quantity of administered fertiliser (corresponding to the driving speed and the number of partial widths) is accomplished using actuators adapted to the conditions of the work environment.

Sulky X40 and X50 spreaders belong to a series that incorporates a Tribord 3Di system on the right spreading disc for remote controlled fertilisation of boundaries. A LINAK actuator shifts the issuing points for the fertiliser to a special shovel for fertilising along boundaries.
Precision and simplicity of control for the Sulky spreader, along with the reliability and accuracy of the LINAK actuator element are thus interlinked.

Contact LINAK TECHLINE for specifications and details on other actuator solutions for spreaders and other farming equipment.

 
Electric actuator solutions -- precise dosing in fertiliser spreaders for increased crop yield play-icon

Electric actuator solutions -- precise dosing in fertiliser spreaders for increased crop yield

Unbreakable play-icon

Unbreakable

Files

Focus on mobile agriculture

This focus folder explains the solutions and benefits that LINAK has provided to the agriculture industry for more than 25 years.

TECHLINE product overview

Explore the wide variety of tough and powerful TECHLINE products. Built to last, built for hard work and built for work in harsh environments.